跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(闪存) 何种情况下可使用闪存复位位?是否可使用读命令中止处理中的其他命令?[2005/03/01]

最新更新:03/01/2005

Question:

(闪存) 何种情况下可使用闪存复位位?是否可使用读命令中止处理中的其他命令?[2005/03/01]

Answer:

闪存复位位用于安全终止擦除与编程命令。为终止命令进程,此位先设为“1”(复位),再设为“0”(正常运行)。
Suitable Products
3803H
3803L
3850A
38D2