跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(串行接口)在UART模式下接收串行I/O数据,什么情况下会发生奇偶校验错误PE或帧错误FE?出错后应怎么处理?

最新更新:10/10/2008

Question:

(串行接口)  在异步(UART)模式下接收串行I/O数据,在什么情况下会发生奇偶校验错误(PE)或帧错误(FE)?出错后,应该如何处理? [2008/10/10]

Answer:

(1)当串行I/O接收允许,奇偶校验允许时(RE = 1 & PARE = 1),如果接收方根据奇偶校验选择位(PARS)计算出的奇偶校验值与接收到的数据中的奇偶校验值不一致,就会产生奇偶校验错误。

(2)当串行I/O接收允许,奇偶校验禁止时(RE = 1 & PARE = 0),奇偶位会被识别为停止位。如果该位的数值不为1,就会发生帧错误。

发生上述问题时的恢复处理,请参照 FAQ 106728。

(#107148)

Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549