跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(串行接口, 调试) 用on-chip仿真器E8调试程序时,是否可以调试UART1?

最新更新:10/10/2006

Question:

(串行接口, 调试) 用on-chip仿真器E8调试程序时,是否可以调试UART1?

Answer:

可以调试这些引脚的除UART1以外的功能(如端口等)。但是,不能调试UART1功能。此外,请勿存取和UART1相关的寄存器。
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L