跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(A/D转换器 )8位分辨率的A/D转换精度如何定义?

最新更新:03/01/2005

Question:

(A/D转换器 )8位分辨率的A/D转换精度如何定义?

Answer:

8位分辨率的A/D转换精度定义如下:

 

(1)相对精度

零过渡电压
表示实际A/D转换输出数据由“0”变为“1”时的模拟输入电压。

满刻度过渡电压
表示实际A/D转换输出数据由“254”变为“255”时的模拟输入电压。

零转移误差= {V0-(1/2) X (VREF/256)}/1LSB [LSB]
表示A/D转换输出数据由“0”变为“1”时,“0~VREF的理想A/D转换特性”的输入电压的偏差。

满刻度转移误差= [V254-{VREF-(3/2) X (VREF/256)}]/1LSB [LSB]
表示A/D转换输出数据由“254”变为“255”时,“0~VREF的理想A/D转换特性”的输入电压的偏差。

线性误差= {Vn-(1LSB X n+V0)}/1LSB [LSB]
表示实际A/D转换特性的“0~V254的理想A/D转换特性”的偏差。

微分非线性误差= {(Vn+1-Vn)-1LSB}/1LSB [LSB]
表示由1改变输出数据所要求A/D转换输入电压的“0~V254的理想A/D转换特性”的偏差。

(2)绝对精度
绝对精度= {Vn-1LSB X (n+1/2)}/1LSB [LSB] 
表示实际A/D转换特性的“0~VREF的理想A/D转换特性”的偏差。

(#104818)

Suitable Products
3803H
3803L
3823
3858
38D2
38D5
7544
3874