跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(A/D转换器 )10位分辨率的A/D转换精度如何定义?

最新更新:03/01/2005

Question:

(A/D转换器 )10位分辨率的A/D转换精度如何定义?

Answer:

10位分辨率的A/D转换精度定义如下:

 

(1)相对精度
零过渡电压
表示实际A/D转换输出数据由“0”变为“1”时的模拟输入电压。

满刻度过渡电压
表示实际A/D转换输出数据由“1022”变为“1023”时的模拟输入电压。

零转移误差= {V0-(1/2) X (VREF/1024)}/1LSB [LSB]
表示A/D 转换输出数据由“0”变为“1”时,“0~VREF的理想A/D转换特性”输入电压的偏差。

满刻度转移误差= [V1022-{VREF-(3/2) X (VREF/1024)}]/1LSB [LSB]
表示A/D转换输出数据由“1022”变为“1023”时,“0~VREF的理想A/D转换特性”输入电压的偏差。

线性误差= {Vn-(1LSB X n+V0)}/1LSB [LSB]
表示实际A/D转换特性的“0~V1022的理想A/D转换特性”的偏差。

微分非线性误差
表示由1改变输出数据所要求输入电压的“0~V1022的理想A/D转换特性”的偏差。

(2)绝对精度
绝对精度= {Vn-1LSB X (n+1/2)}/1LSB [LSB]
表示实际A/D转换特性的“0~VREF的理想A/D转换特性”的偏差。

Suitable Products
3803H
3803L
3823
3850A
38D2
38D5
7546
7547
7548
7549
3874