跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(A/D转换器 )执行STP指令时,A/D转换器的状态如何?

最新更新:03/01/2005

Question:

(A/D转换器 )执行STP指令时,A/D转换器的状态如何?

Answer:

执行STP指令时,A/D转换器处于停止模式。因此,务必在完成A/D转换后,执行STP指令。即使MCU在A/D转换过程中进入停止模式,电流将继续流入A/D转换器。从停止模式返回后,转换结果不确定。
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549