跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

(定时器)定时器2和定时器LC计数开始定时,且在操作开始后进行计时。 [2005/01/17]

最新更新:01/17/2005

Question:

(Timer)   Timer 2 and timer LC count start timing and count time when operation starts. [2005/01/17]

Answer:

 

Count starts from the rising edge (2) after the first falling edge of the count source, after timer 2 and timer LC operations start (1).
Subject to the operation start timing of the timers and count source, after count starts, the time to the first underflow (3) will be different from the time between subsequent underflows (4). (#105078)

Suitable Products
4559
455A