跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

通过串行I/O写入闪存数据时,需集成串行I/O控制程序在CPU可再编程模式控制程序中吗?

最新更新:03/01/2005

Question:

(闪存) 通过串行I/O写入闪存数据时,需集成串行I/O控制程序 在CPU可再编程模式控制程序中吗?[2005/03/01]

Answer:

是的。除此之外,还需初始化端口、禁止中断与写入看门狗定时器等。
Suitable Products
3803H
3803L
3850A
38D2