跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

未用端口的处理中为什么P12_0(XIN)引脚和P12_1(XOUT)引脚需要经电阻连到VCC(上拉)?能进行下拉处理?

最新更新:10/03/2008

Question:

(I/O 端口, 引脚) 在未使用端口的处理中,为什么P12_0(XIN)引脚和P12_1(XOUT)引脚需要通过电阻连接到VCC(上拉)?如果进行下拉处理行吗?

Answer:

复位后,引脚P12_0(XIN)和P12_1(XOUT)仍处于输入状态,所以对两个引脚进行下拉,也没有问题。
“在未使用引脚P12_0(XIN)和P12_1(XOUT)时,硬件手册推荐进行上拉处理的原因”是:当引脚P12_0(XIN)和 P12_1(XOUT)未使用时,万一把XIN-XOUT引脚设为时钟振荡,高电平信号将从XOUT引脚输出。此时,如果两个引脚为下拉处理,那么在MCU内部将有电流流经XIN引脚,一般会导致几μA电流的增加。因此,推荐进行上拉处理。
Suitable Products
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC