跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

当VREF与VCC不同,将部分与A/D复用的引脚作为输出端口使用时,输出的高电平是VREF还是VCC?

最新更新:10/10/2008

Question:

(A/D转换器, I/O端口)  当VREF与VCC不同,将部分与A/D转换器复用的引脚作为输出端口使用时,输出的高电平是VREF还是VCC? [2008/10/10]

Answer:

输出的高电平是VCC。 (#107142)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547