跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

关于uPD78054系列产品的串行接口控制寄存器0的时钟选择方法,应对8位定时器2执行何种设置?

最新更新:2011年10月 06日

Question:

关于uPD78054系列产品的串行接口控制寄存器0的时钟选择的方法,我应该对8位定时器2执行什么样的设置?甚至当我将CSIM0设置为9AH时,时钟也不能从SCK0产生。

Answer:

不能通过简单的设置CSIM0来实现时钟从SCK0输出。
下面这些初始化的设置是必须的:

- 为了从SCK0输出一个时钟,除设置CSIM0之外,将PM27设置为0(输出),并将P27设置为1。
- 对于CSIM0的设置,SB1和SCK0引脚必须接上拉电阻。


当发送的数据被写到SIO0,或者在接收的情况下,0FFH在这个状态下被写到SIO0时, 通讯应该开始,且SCK0也应该被输出。

Suitable Products
  • 这篇文章对您有帮助吗?