跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

关于QzROM出货 根据数据表,ROM代码保护地址是FFDBh,但在QzROM写确认书中是10h,为何?

最新更新:11/05/2008

Question:

(QzROM) 关于QzROM出货
(1)根据数据表,ROM代码保护地址是 FFDBh,但是在QzROM写确认书中是10h,如何解释?
(2)根据ROM选项数据,若FFDBh设定为其他数据(如FFh),但是00h写入ROM选项,会出现何种情况?
(3)是否可以读取QzROM保护区域的数据?

Answer:

(1)ROM代码保护区域分配到单片机的FFDBh 地址。ROM选项数据(10h)的地址并不是芯片的0010h地址,是指掩模文件转换工具(MM)使用(在掩模转使用时为“掩模选项建立”)时的ROM选项建立地址(请查阅掩模文件转换工具使用用户手册16页)。
(2)只要00h设定到ROM选项,即使其他数据设定为FFDBh,依照ROM选项数据的内容,并保护所有ROM代码的区域。
(3)不可以,不能读取保护ROM数据。
Suitable Products
3803H
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549