跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

从模式被选定,SSE1=0(不使用)被设置时,可否进行正常的接收操作? 一个传送操作能否通过写STOB1来启动?

最新更新:2011年10月 06日

Question:

当从模式被选定,SSE1 = 0 (不使用)被设置时,可以进行正常的接收操作吗?
一个传送操作能否通过写STOB1来启动?

Answer:

当 SSE1 = 0 时,执行正常的3线操作。
甚至在正常的从操作期间,发送也不能简单的通过向STOB1写数据启动。
在这个案例中,在向STOB1写完数据之后,只有当来自主设备的时钟被输入时,才启动发送。
Suitable Products