跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

为何内部输出电阻R0是4kΩ?R0是否通常都是4kΩ?R0=4kΩ是否仅作为一个例子?

最新更新:03/13/2008

Question:

(D/A转换器) 38000系列D/A转换器,FAQ103072的答案如下:
“例如,D/A输出3V,若运算放大器的输入电阻是无限大的,内部输出电阻R0是 4kΩ,DAi引脚电平如下:
3[V] X 100kΩ/(100kΩ + 4kΩ) = 2.885[V].”
(1)为何内部输出电阻R0是 4kΩ?R0是否通常都是 4kΩ?R0 = 4 kΩ是否仅作为一个例子?
(2)D/A输出引脚和R-2R电阻器之间的电阻是否为“内部输出电阻器R0”?

Answer:

(1) R0 = 4 kΩ仅是一个例子。
(2)是的,内部输出电阻R0是R-2R 和D/A输出引脚的合并电阻。

(#106877)

Suitable Products
3803H
3803L