跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

串行I/O2控制寄存器和方向寄存器,对于串行I/O2端口选择位的P45/SOUT2与P46/SCLK2引脚功能有何影响?

最新更新:04/18/2005

Question:

(串行接口) 串行I/O2控制寄存器(SIO2CON)和方向寄存器,对于串行I/O2端口选择位(位3)的P45/SOUT2引脚与P46/SCLK2引脚功能有何影响? [2005/04/18]

Answer:

当位3为1时,不考虑方向寄存器的设定情况,串行 I/O2 同步时钟选择位(位6)的 P45/SOUT2引脚与P46/SCLK2引脚具有以下功能。()表示方向寄存器-0时,读取端口的值。
位6=0时: SOUT2 输出引脚(“1”),SCLK2输入引脚(引脚状态)。
位6=1时:SOUT2 输出引脚(数据发送中“1”,发送后数据状态),SCLK2输出引脚(“1”)。
当位3为0时,P45/SOUT2 引脚为I/O端口P45,P46/SCLK2 引脚为I/O端口P46。

(#105190)

Suitable Products
38D5