跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

中断优先级选择位(为0,并且中断请求位(IR)为1时,若设定ILVL0-ILVL2为7,会执行中断程序吗?

最新更新:10/10/2006

Question:

(中断) 中断优先级选择位(ILVL0-ILVL2)为“0”(禁止中断),并且中断请求位(IR)为“1”(有中断请求)时,若设定ILVL0-ILVL2为“7”(中断:允许;中断优先级:最高优先级),是否执行中断程序?

Answer:

若中断标志(I标志)为“1”(允许),则执行中断程序。但是,不可屏蔽中断或其它ILVL0-ILVL2为“7”的中断(是否在执行中等情况)会影响执行时序。
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC