跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Will the timer recount if the STR bit of the CMSTR is set to "1"?

Latest Updated:04/01/2010

Question:

When the compare match timer CMT) is counting(when the STR bit is "1"), if the STR bit of the compare match timer start register(CMSTR) is set to "1"(count operation), will the timer recount?

Answer:

No, even if the STR bit is set to "1" during counting, the timer will not recount.
This setting is disregarded and the counting continues.
Suitable Products
SH7144, SH7145
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7018
SH7014, SH7016, SH7017
SH7011