跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

When I reset, output of RTCOUT stops.

Latest Updated:05/28/2013

Question:

When I reset, output of RTCOUT stops.

Answer:

Due to the reset, the registers become the "values after reset". Set the following registers again.
- RTCOUT output control bit (RCR2.RTCOE)

Suitable Products
RX62N, RX621
RX630
RX63N, RX631
RX210
RX220
RX110
RX111