跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Omission of SCI Transmission Data Byte

Last Updated:07/04/2018

Question:

SCI transmission data is partly omitted. What could be the reasons and how to fix it?

Answer:

Make sure that the TDR register is not written with new data before the  transmission buffer register becomes empty.
Suitable Products
RX Family
  • 这篇文章对您有帮助吗?