跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

Communication Using Multiple Channels for SCI FIT

Last Updated:07/04/2018

Question:

For SCI module Firmware Integration Technology (FIT), when using multiple channels, the channels set after the first one do not start communication. What could be the reasons and how to fix it?

Answer:

Check if the SCI FI API return value is an error. 
When SCI_ERR_QUEUE_UNAVAILABLE is returned as a return value to the  R_SCI_Open function, the number of buffers saved in the BYTEQ module are not enough.
Change the BYTEQ_CFG_MAX_CTRL_BLK setting value of the configuration header file in the ByteQ module.
Suitable Products
RX Family
  • 这篇文章对您有帮助吗?