跳转到主内容
Knowledgebase
Home
Renesas Electronics China - Knowledgebase

What Happens to INTAD Flag If ADCS=1 Is Written Just Before Completion of A/D Conversion

Last Updated:05/25/2018

Question:

What will happen to INTAD flag if ADCS=1 is written just before the A/D conversion operation is completed?

Answer:

If "1" is written into ADCS before the A/D conversion operation is completed, INTAD (A/D conversion completion interrupt) does not occur and the A/D conversion is re-executed from the start. Afterwards, when the A/D conversion is completed, INTAD will occur.
Suitable Products
RL78/G10
RL78/G11
RL78/G12
RL78/G13
RL78/G14
RL78/G1A
RL78/G1C
RL78/G1D
RL78/G1E
RL78/G1F
RL78/G1G
RL78/G1H
RL78/I1A
RL78/I1C
RL78/I1D
RL78/I1E
RL78/L12
RL78/L13
RL78/L1A
RL78/L1C
78K Family